DDR Introduction
This document describes how to create a new DDR configuration and configure the DDR component using the DDR Configuration and Validation Tool.
|
|
DDR Tool is a Windows and Linux based software to help users to execute LPDDR4/DDR3L training, stress test and DDR initialization. Generated code can be used within u-boot as it follows u-boot coding style. ATF and MISRA formats are also available under Code Format option.
Currently supported memory types are:
- LPDDR4 (JEDEC 209-4A)
- DDR3 (JEDEC JESD79-3F)