Exporting sources

It's possible to export the generated source using the Export wizard.

To launch the Export wizard:
  1. Select File > Export from the Menu bar.
  2. Select Export Source Files.
    Figure 1. Export wizard
  3. Click Next.
  4. Select the target folder where you want to store the generated files.
    Figure 2. Select target folder
  5. In case of multicore processors, select the cores you want to export.
  6. Click Finish.