Full initialization of pins

In some cases, the default values are not reliable, as there may be code running before the application that modifies the pin configuration (for example, a bootloader). The option Full initialization of pins ensures that the initialization is fully done even for items that use after-reset state. This option is specific for each Functional group allowing to force full initialization of routing. Full initialization of pins is not enabled by default. When enabled, the electrical properties of existing routing are changed. The "Reset" values are changed to explicit values corresponding with them. When the option is disabled, the pins tool changes the values that are matching after-reset state to the "Reset" values.