Functional groups
These groups represent functions which will be generated into source code.
Use the dropdown menu to switch between functional groups and configure them.
You can use two additional buttons to further configure functional groups:
| Icon | Description |
|---|---|
![]() |
Toggle "Called from default initialization function" feature (in source code) |
![]() |
Opens the Functional group properties window |
Note:
Red/orange background indicates errors/warnings in the configuration.