Problems view

The Problems view displays issues in individual tools and in the inter-dependencies between the tools.
Figure 1. Problems view

To open the Problems view, click the Show Problems view button in the Toolbar, or select Views > Problems from the Menu bar.

The Problems table contains the following information:
Table 1. Problems view
Item Description
Level Severity of the problem: Information, Warning, or Error.
Resource Resource related to the problem, such as signal name, the clock signal.
Issue Description of the problem.
Origin Information on the dependency source.
Target Tool that handles the dependency and its resolution.
Type Type of the problem. It is either the validation checking dependencies between tools, or a single tool issue.
Every issue comes with a context menu accessible by right-clicking the table row. Use this menu to access information about the problem or to apply a quick fix where applicable. You can also copy the rows for later use by right-clicking the row and selecting Copy or by using the Ctrl+C shortcut. You can use the Ctrl+left-click shortcut to add additional rows to the selection.
Note: Quick fix is only available for problems highlighted with the "light bulb" icon.