Overview

Trace Commander feature uploads the trace and configures the modules included in the target architecture in a more user-friendly graphical interface.

For S32V234, the Trace IP looks like this:

Figure 1. S32V234 Trace IP


The 4 A53-cores of the S32V234 are split in 2 clusters, each with 2 cores. Core 0 and Core 1, from Cluster 0, output trace in ETF 0 and Core 2 and Core 3, from Cluster 1, store trace in ETF 1. You can only collect from one ETF at a time.

Note: For some platforms, trace is not supported for all cores.