SDK Explorer view

The SDK Explorer view displays the structure of SDKs belonging to the active project.

To open the SDK Explorer view, click Window > Show View > Other. In the Show View dialog box, expand the Other section and select SDK Explorer . Click OK.

Select any project file or folder in Project Explorer. The SDK Explorer displays the include folder for each SDK attached to the project, with nested folders and header files inside:


SDK Explorer view

You can perform the following actions in the SDK Explorer view: