Attaching an SDK when creating a project

When creating a new project, you have an option to add an SDK on the second page of the wizard. Click the ellipsis button in the SDKs field. In the Select SDK dialog box, flag SDKs to be selected from the list and click OK.


SDK selection in S32DS Application Project wizard

The Select SDK dialog box displays both predefined and custom SDKs that are compatible with the project's language, target processor, toolchain, and core.