All project examples are available for use in the S32DS Project from Example wizard. To open the wizard, click .
The User Examples section of the S32DS Project from Example wizard is reserved for project examples added by the user. To add a project to User Examples, copy the project folder from your workspace to the {S32 Design Studio for S32 Platform 3.5 Update 6 RTM installation path}/S32DS/examples folder.An example can include several projects. For instance, when you design an application for a multi-core processor, you use a separate application project for each core. You can pack all these projects into one example. When someone decides to use your example, they install all included projects to the workspace.
To add a multi-project example to User Examples:
Now the S32DS Project from Example wizard displays your example under User Examples.

The example is located in the upper-level folder that you copied or created in the /S32DS/examples folder.