The Arm System Registers view provides the structured view of the Arm System registers (if available) of the target hardware.
The Arm System Registers view is included in the Debug perspective by default. If the view was closed, reopen it from the menu by selecting .

The Arm System Registers view presents the information about the Arm System registers in a tabular format. The Peripherals column displays the registers arranged in a hierarchy with the following levels (from top to bottom): a group of registers, a peripheral, a cluster (if set), a register, a field (sequential bits within a register). Any node in the hierarchy can be expanded or collapsed with a click.
The Description column provides the information about the object shown in the Registers column.
The toolbar of the Arm System Registers view includes the following buttons (from left to right):
![]() |
(Show structure) | Toggle for the Arm System Registers view to show registers combined in categories. |
![]() |
(View Menu) | Click to open the menu customizing the layout of the
Arm System Registers view. Options:
|
![]() |
(Minimize) | Click to minimize the Arm System Registers view. |
![]() |
(Maximize) | Click to maximize the Arm System Registers view. All other views are minimized and their icons appear at the right border of the main application window, each next to the dedicated Restore icon. |
![]() |
(Restore) | Click to restore the Arm System Registers view from minimal or maximal state. |