The Migrate wizard assists you in migrating projects to new SDK or toolchain available.
The availability of migrations depends on the installed packages.

The following table describes the settings that you can configure.
| Option | Description |
|---|---|
| Projects | Shows the available projects. Note: If opened from the Project
Explorer, the corresponding projects will be
selected.
Note: Multiselection is available.
|
| Available migrations | The availability of migrations depends on Projects selection (project type based). |
| Details | Brief information on the selected migration to be performed. |
| Create backup | Enable this option to create a backup of your project. |
| File | The location where the project backup will be stored. Click
Browse button to select location and filename. If Create backup checkbox is clear, this field is inactive. The Browse button and backup properties selection are inactive. |
| Backup format | Backup archive type selection. Options:
|
| Compress the content | Enable this option to compresses the contents in the archive that is created. |
| Backup linked resources | Enable this option to backup project with all linked resources. |