S32DS Project from Example wizard

The S32DS Project from Example wizard creates a new project on the basis of a project sample. The new project includes all files of the sample project.

To launch the S32DS Project from Example wizard, click File > New > S32DS Project from Example on the menu bar.


S32DS Project from Example

UI control Description
Project name field Automatically displays the name of the selected sample project. The displayed name can be edited.
Note: The field is empty and cannot be edited until a sample project is selected in the Examples pane.
Search box Serves for quick search in the Examples pane.
Hardware Filter button Serves for quick search of projects for certain devices in the Examples pane.
Note: If there are some device specific examples available but a corresponding device package is not installed, the hardware is indicated as Undefined.
Examples pane Displays sample projects arranged in sections.

The User Examples section is empty by default. This section is reserved for sample projects created by the user. Find the details in Saving a project to User Examples.

Projects in the remaining sections are installed with S32 Design Studio .

Description pane Displays the information about the project currently selected in the Examples pane. This information may be missing.
Finish button Saves a copy of the selected project with the specified project name. The new project is displayed in the workspace for editing and debugging.