Peripheral Registers view

The Peripheral Registers view provides the structured view of the peripheral registers on the target hardware. If Arm® core registers are defined for the target device they are also present in this view.

The Peripheral Registers view is included in the Debug perspective by default. If the view was closed, reopen it from the menu by selecting Window > Show View > Other > Debug > Peripheral Registers.


Peripheral Registers view

The Peripheral Registers view presents the information about the peripheral registers in a tabular format. The Peripherals column displays the registers arranged in a hierarchy with the following levels (from top to bottom): a group of registers, a peripheral, a cluster (if set), a register, a field (sequential bits within a register). Any node in the hierarchy can be expanded or collapsed with a click.

The Description column provides the information about the object shown in the Peripherals column.

The remaining columns are populated for the “register” nodes:

The toolbar of the Peripheral Registers view includes the following buttons (from left to right):

(Show structure) Toggle for the Peripheral Registers view to show peripheral registers combined in categories.
(View Menu) Click to open the menu customizing the layout of the Peripheral Registers view. Options:
  • Restore table layout: Sets the layout to its default.
(Minimize) Click to minimize the Peripheral Registers view.
(Maximize) Click to maximize the Peripheral Registers view. All other views are minimized and their icons appear at the right border of the main application window, each next to the dedicated Restore icon.
(Restore) Click to restore the Peripheral Registers view from minimal or maximal state.
The Peripheral Registers view context menu has the following options: