To let you edit a device configuration, S32 Design Studio provides perspectives named Pins, Clocks, Peripherals, DCD (Device Configuration Data), IVT (Image Vector Table), QuadSPI and DDR. The settings that you edit and save in these perspectives are automatically stored in the configuration file of the currently used project.
(Open S32
Configuration) button on the toolbar. Click to open the required perspective.

The use of settings in the perspectives is beyond the scope of this document. You can read more about the subject in the S32 Configuration Tools Getting Started guide. To open this guide, click on the menu.
While configuring your processor, you can switch between the perspectives using the
(Open
S32 Configuration) toolbar button.
To save the changes to the project, use the Update Code toolbar button. A click on this button either saves the latest device configuration silently or opens the Update Files dialog box.
When saving the changes for the first time, click .

In the Update Files dialog box, select the device configuration files to be created in the project and updated with the latest pin, clock, peripheral and other settings:

You can configure the Update Code button to always open the Update Files dialog box or not. To do it, select or deselect the Always show details before Update Code option in the Update Files dialog box, then click OK.