Exporting a project to a system folder or an archive file

To export a project to a system folder or to a ZIP or TAR archive file:

  1. Right-click the project in the Project Explorer and click Export on the context menu.
  2. In the Export wizard, go to General and select Archive File or File System as the destination for export. Click Next.


    Exporting a project

  3. On the next wizard page, do the following:
    • In the left pane, remove flags from the project folders that you want to be excluded from export. Click a folder in the left pane to see all included files in the right pane. Remove flags from the project files to be excluded from export.
    • Browse to the destination folder or archive file, or enter the path manually. If the specified folder or archive file does not exist, it will be created during export.
    • Specify the options for export.
  4. Click Finish.