If you need to take control of operations with flash memory during debugging, you can do it using the flash programmer tool delivered with S32 Design Studio . This tool enables read-write access to QSPI flash memory of the connected target. All operations are performed from the command line.