You can use the Migrate wizard
to convert SDK or GCC based tolchain for your project.
Note: Generally the SDK migration contains a toolchain migration in it.
Note: For toolchain migration refer steps 1-5 only.
The following explains how to migrate your project:
If the selected toolchain is not supported in the
New Project
wizard for the processor type of the original project, the migrated project may contain
some errors.
If system generates any errors or warnings, you can see them in the
Problems view. You can use the Quick
Fix option if possible.