Using optional tools

A build configuration can include optional tools such as:

To be executed at build time, these tools need to be enabled and set up in the build configuration. Find an example in topic Generating an image file.

Also, a build configuration includes tools that are never called at build time: You can call these tools from the menu for the selected project files. Find the details in topics Preprocessing source files and Disassembling binaries and source files.