Command-line execution - DCD Tool
This section describes the Command Line Interface (CLI) commands supported in the DCD Tool.
| Command name | Definition and parameters | Description | Restriction | Example |
| Import DCD binary image | -ImportBin |
Import the binary DCD image in the current configuration. The path of the imported binary image is expected as argument. |
Requires -HeadlessTool DCD | -HeadlessTool DCD -ImportBin C:/boot_images/dcdImg.bin |
| Export DCD image in binary format | -ExportBin |
Export the DCD image in binary format. Folder name is expected as argument. |
Requires -HeadlessTool DCD | -HeadlessTool DCD -ExportBin C:/exports/generated |
| Export DCD image in C format | -ExportC |
Export the DCD image in C format. Folder name is expected as argument. |
Requires -HeadlessTool DCD | -HeadlessTool DCD -ExportC C:/exports/generated |
|
Export all generated files (to simplify all export commands to one command) |
-ExportAll |
Export generated files (with source code etc.). Code will be regenerated before export. Includes -ExportBin,-ExportC and in framework -ExportMEX. Folder name is expected as argument. |
Requires -HeadlessTool DCD | -HeadlessTool DCD -ExportAll C:/exports/generated |
|
Validate configuration |
-ValidateConfiguration |
Validates the current loaded configuration and display the problems found. |
Requires -HeadlessTool DCD | -HeadlessTool DCD -Load C:/mex_files/myMex.mex -ValidateConfiguration |
- Import DCD binary image and save it to C format:
eclipsec.exe -noSplash \-application com.nxp.swtools.framework.application \--launcher.ini /path/to/S32DS/installation/eclipse/s32ds.ini \-HeadlessTool DCD \-MCU /processor/name \-SDKVersion /sdk/version/name \-ImportBin /path/to/dcd/binary \-ExportC /path/where/to/save/fileOR
eclipsec.exe -noSplash \-application com.nxp.swtools.framework.application \--launcher.ini C:\NXP\S32DesignStudio\eclipse\s32ds.ini \-HeadlessTool DCD \-MCU S32S247TV \-SDKVersion s32sdk_s32s_rtm_100 \-ImportBin C:\Input\dcd_image.bin \-ExportC C:\Output - Export all DCD binaries based on a .mex
file:
eclipsec.exe -noSplash \-application com.nxp.swtools.framework.application \--launcher.ini /path/to/S32DS/installation/eclipse/s32ds.ini \-HeadlessTool DCD \-Load /path/to/mex/file\-ExportAll /path/where/to/save/files - Validate configuration based on existing .mex file and report
errors:
eclipsec.exe -noSplash \-application com.nxp.swtools.framework.application \--launcher.ini /path/to/S32DS/installation/eclipse/s32ds.ini \-HeadlessTool DCD \-Load /path/to/mex/file \-ValidateConfiguration