Command-line execution - Peripherals Tool

This section describes the Command Line Interface (CLI) commands supported by the Peripherals Tool.

Table 1. Commands supported in Peripherals Tool
Command name Definition and parameters Description Restriction Example
Enable tool -Enable

Enables the tool if it is disabled in the current configuration.

​Requires -HeadlessTool Peripherals -HeadlessTool Peripherals

-Enable

Import C files

-ImportC

Imports .c files into the configuration.

Importing is done after loading mex and before generating outputs.

Requires -HeadlessTool Peripherals -HeadlessTool Peripherals

-ImportC C:/imports/file1.c C:/imports/file2.c

​​Export all generated files

(to simplify all exports commands to one command)

​​-ExportAll

​Exports generated files (with source code and so on)

The code is regenerated before the export.

Includes -ExportSrc, -ExportHTML, and in framework -ExportMEX

The argument is expected to be a folder.

​Requires ​​-HeadlessTool​ Peripherals -HeadlessTool​ Peripherals ​

-ExportAll C:/exports/generated
​​Export Source files ​-ExportSrc​

Exports generated source files.

The code is regenerated before the export.

The argument is expected to be a folder.

​Requires ​​-HeadlessTool​ Peripherals ​​​-HeadlessTool​ Peripherals

-ExportSrc C:/exports/src​
Export the HTML report file -ExportHTML

Exports the generated HTML report file.

The code is regenerated before the export.

The argument is expected to be a folder.

Requires -HeadlessTool Peripherals -HeadlessTool Peripherals

-ExportHTML C:/exports/html
Migrate all Peripherals tool components to the versions used in toolchain project ​-Migrate

Components

To

ToolchainVersion
​Migrates all instances of Peripherals tool components, which are not configuring the version used in the toolchain project, to the version of SDK component used in toolchain project. No changes are done when toolchain is not linked or the Peripherals tool component already configures the version of the SDK component used in the toolchain project. ​Requires -HeadlessTool Peripherals ​-HeadlessTool Peripherals -MigrateComponentsToToolchainVersion -ExportAll C:/exports/toolchainVersions
​​Migrate all Peripherals tool components to the highest supported version of the SDK component ​​-MigrateComponents

To

LatestVersion
​Migrates all instances of Peripherals tool components to the MCU's highest supported version of the SDK component, which the Peripherals tool component configures. No changes are done when already using the highest version available on the MCU. ​Requires -HeadlessTool Peripherals ​-HeadlessTool Peripherals -MigrateComponentsToLatestVersion -ExportAll C:/exports/toolchainVersions
​Regenerate all PLU configurations ​-PLURegenerate

Configurations
​Regenerates content of all PLU instances present in the configuration. Currently only the PLU instances in Verilog file and Verilog text modes are regenerated by new Verilog code synthesis and optimization of the model. Requires usage of mapping comment in the Verilog code. ​Requires -HeadlessTool Peripherals ​-Load C:/xyz.mex

-HeadlessTool Peripherals -PLURegenerateConfigurations

- ExportAll C:/exports/plu
Examples:
  • Generate code and export configuration in .mex file and HTML format:
    eclipsec.exe -noSplash \
            -application com.nxp.swtools.framework.application \
            --launcher.ini /path/to/S32DS/installation/eclipse/s32ds.ini \
            -HeadlessTool Peripherals \
            -MCU /processor/name \
            -SDKVersion /sdk/version/name \
            -ExportMEX /path/where/to/export/file \
            -ExportHTML /path/where/to/export/file

    OR

    eclipsec.exe -noSplash \
            -application com.nxp.swtools.framework.application \
            --launcher.ini C:\NXP\S32DesignStudio\eclipse\s32ds.ini \
            -HeadlessTool Peripherals \
            -MCU S32S247TV \
            -SDKVersion s32sdk_s32s_rtm_100 \
            -ExportMEX C:\Output \
            -ExportHTML C:\Output
  • Import configuration from existing .mex file and generate code:
    eclipsec.exe -noSplash \
            -application com.nxp.swtools.framework.application \
            --launcher.ini /path/to/S32DS/installation/eclipse/s32ds.ini \
            -HeadlessTool Peripherals \
            -Load /path/to/mex/file \
            -ExportSrc /path/where/to/export/generated/files