Command-line execution - Pins Tool
This section describes the Command Line Interface (CLI) commands supported in the Pins Tool.
| Command name | Definition and parameters | Description | Restriction | Example |
|---|---|---|---|---|
| Enable tool | -Enable | Enables the tool if it is disabled in the current configuration | Requires -HeadlessTool Pins | -HeadlessTool Pins -Enable |
| Import C files | -ImportC |
Imports .c files into configuration Importing is done after loading mex and before generating outputs |
Requires -HeadlessTool Pins | -HeadlessTool Pins -ImportC C:/imports/file1.c C:/imports/file2.c |
|
Export all generated files (to simplify all exports commands to one command) |
-ExportAll |
Exports generated files (with the source code, and so on) The code is regenerated before the export. Includes -ExportSrc,-ExportCSV, -ExportHTML and in framework -ExportMEX The argument is expected to be a folder |
Requires -HeadlessTool Pins | -HeadlessTool Pins -ExportAll C:/exports/generated |
| Export Source files | -ExportSrc |
Exports generated source files. The code is regenerated before the export. The argument is expected to be a folder. |
Requires -HeadlessTool Pins | -HeadlessTool Pins -ExportSrc C:/exports/src |
| Export CSV file | -ExportCSV |
Exports the generated .csv file. The code is regenerated before export. The argument is expected to be a folder. |
Requires -HeadlessTool Pins | -HeadlessTool Pins -ExportSrc C:/exports/src |
| Export HTML report file | -ExportHTML |
Exports the generated HTML report file. The code is regenerated before the export. The argument is expected to be a folder. |
Requires -HeadlessTool Pins | -HeadlessTool Pins -ExportHTML C:/exports/html |
| Export registers | -ExportRegisters |
Exports the registers tab into a folder. The code is regenerated before the export. The argument is expected to be a folder. |
Requires -HeadlessTool Pins | -HeadlessTool Pins -ExportRegisters C:/exports/regs |
- Import
configuration from C file and export full list of
registers:
eclipsec.exe -noSplash \-application com.nxp.swtools.framework.application \--launcher.ini /path/to/S32DS/installation/eclipse/s32ds.ini \-HeadlessTool Pins \-MCU /processor/name \-SDKVersion /sdk/version/name \-ImportC /path/to/C/file \-ExportRegisters /path/to/file/where/to/export/registersOR
eclipsec.exe -noSplash \-application com.nxp.swtools.framework.application \--launcher.ini C:\NXP\S32DesignStudio\eclipse\s32ds.ini \-HeadlessTool Pins \-MCU S32S247TV \-SDKVersion s32sdk_s32s_rtm_100 \-ImportC C:\Input\pin_mux.c \-ExportRegisters C:\Output - Import configuration from existing .mex file and generate
code:
eclipsec.exe -noSplash \-application com.nxp.swtools.framework.application \--launcher.ini /path/to/S32DS/installation/eclipse/s32ds.ini \-HeadlessTool Pins \-Load /path/to/mex/file \-ExportSrc /path/where/to/save/generated/files