Beginning with pin/internal signal selection

You can select a pin or an internal signal in the Routing Details view.
  1. Select the pin/internal signal (Routed pin/signal).
  2. Select one of the available Peripherals.
  3. For the selected peripheral, select one of the available Signals.
    Items in the Peripheral column in the Routing Details view have the following symbols:
    • The exclamation mark and default text color indicate that such item selection can cause a register conflict or the item does not support the selected signal.
    • The exclamation mark and gray text color indicate that the item cannot be routed to the selected pin/internal signal. The item is available for different pin/internal signals using the same signal.
      Note: In the Pins view and the Package view, you can configure only pins and not internal signals.