Clock sources
The Clock Sources table is in the Clocks Table view. You can also edit the clock sources directly from the Diagram view or from the Details view.
You can configure the availability of external clock sources (check the checkbox) and set their frequencies. Some sources can have additional settings available when you unfold the node.
If the external crystal or the system oscillator clock is available, check the
checkbox in the clock source row and specify the frequency.
|
|
Note: Some clock sources remain inactive even though the checkbox is
checked. It is because the clock sources functionality depends on other settings like power
mode or additional enable/disable setting options. You can hover the cursor on the setting
to see a tooltip with information on the element and possible limitations/options.