Clocks menu
Options related to the Clocks tool can be found in the Clocks menu in the Menu bar.
| Menu item | Description |
|---|---|
| Functional groups | Open the Functional group properties dialog. |
| Refresh | Refresh each clocks configuration with explicit invocation of code generation. |
| Reset To Board Defaults | Reset the clock model to board defaults. |
| Reset To Processor Defaults | Resets the clock model ito processor defaults. |
| Unlock All Settings | Unlocks all locks in all settings. |
| Unlock Settings on the Active Path | Unlocks all locks in the settings that are on the active path. |