Code Generation

If the settings are correct and no error is reported, the code generation engine instantly regenerates the source code. You can view the resulting code the Code Preview view of the DCD tool.

Code Preview automatically highlights differences between the current and immediately preceding iteration of the code. You can choose between two modes of highlighting by clicking the Set viewing style for source differences. You can also disable highlighting altogether from the same dropdown menu.
Figure 1. Code Preview