Code Generation
If the settings are correct and no error is reported, the code generation engine instantly regenerates the source code. You can view the resulting code the Code Preview view of the DCF tool.
Code Preview automatically highlights differences between the current and
immediately preceding iteration of the code. You can choose between two modes of
highlighting by clicking the Set viewing style for source differences. You can
also disable highlighting altogether from the same dropdown menu.
|