Config tools overview

The Config Tools Overview provides you with general information about your currently active configuration, hardware, and project. It also provides a quick overview of the used/active and unused/inactive tools, generated code, and functional groups. By default, the Config Tools Overview icon is on the left side of the toolbar.

Config Tools Overview contains several items.
Table 1. Config Tools Overview
Item Description
Configuration – General Info Displays the name of and the path to the MEX file of the current configuration. Click the link to open the folder containing the MEX file. To import additional settings, click the Import additional settings into current configuration button.
Configuration – HW Info Displays the processor, part number, core, and SDK-version information of the current configuration.
Project Displays toolchain project information.
To enable/disable the tools, click the toggle button. You can navigate to the tools by clicking their icons. The following information about the tools is also available:
Table 2. Config Tools Overview
Item Description
Generated code Contains the list of source-code files. Click the links to open the files in the Code Preview view.
Functional groups Contains the list of the currently active functional groups. To select the groups in the Functional groups tab in the toolbar, select the relevant links.
  • Figure 1. Config Tools Overview
    Note: Unsupported tools are not displayed in the overview.