DCF Commands View

Commands view is the graphical interface that displays the complete sequence of commands for the DCF image. The commands can be rearranged using drag and drop.

Figure 1. DCF Commands View

To get a better overview of the current commands, the user can toggle the Minimized view using the button on the upper-left part of the view.

Figure 2. Minimized Commands View