DDR html report

DDR Tool generates an html report of the training parameters and mode registers settings that can be stored by the customer along with the generated code, using the Update Code feature.

The report contains three main sections :

  • General Information - This section contains details about the general settings of the current configuration. It supports the DDR Type (e.g. LPDDR5) and the Firmware Version (e.g. 2023_10).
  • UI Configuration - A representation of the DDR View’s UI parameters in a similarly shaped tree viewer with interactive collapsible nodes. It represents a snapshot of the visible DDR parameters configuration. Any change in the DDR UI should also be reflected automatically in this report.
  • Registers Tables - A list of custom registers tables with detailed information about their bitfields values.
Figure 1. DDR html report