Errors and warnings

The Pins Tool checks for any conflict in the routing and also for errors in the configuration. Routing conflicts are checked across all INIT functions (default initialization functions). It is possible to configure different routing of one pin in different functions (not INIT functions) to allow dynamic pins routing reconfiguration.
If an error or warning is encountered, the conflict in the Routing Details view is represented in the first column of the row and the error/warning is indicated in the cell, where the conflict was created. The detailed error/warning message appears as a tooltip.

For more information on error and warnings color, see the Highlighting and Color Coding section.