Exporting the Pins table

To export the Pins table, do the following:
  1. In the Menu bar, select File > Export.
  2. In the Export wizard, select Export the Pins in CSV (Comma Separated Values) Format.
    Figure 1. Export dialog
    Figure 2. Export dialog
  3. Click Next.
  4. Select the folder and specify the filename to which you want to export.
    Figure 3. Export the Pins in CVS
  5. The exported file contains content of the Pins view table, and lists the functions and the selected routed pins.
    Figure 4. Exported file content
The exported content can be used in other tools for further processing. For example, see it after aligning to blocks in the image below.
Figure 5. Aligning to block