Functional groups
These groups represent functions that will be generated into the source code. Use the
dropdown menu to switch between functional groups and configure them.
|
You can use two additional buttons to further configure functional groups:
| Icon | Description |
|---|---|
![]() |
Toggle "Called from default initialization function" feature (in source code) |
![]() |
Opens the Functional group properties window |
Note:
Red/orange background indicates errors/warnings in the configuration.