GTM Diagram View
The interactive diagram provide an overall overview of the GTM configuration in which certain essential attributes of the configuration are displayed.
The GTM Diagram view contains two areas: toolbar area and diagram area.
The toolbar contains controls to interact with diagram :
- navigation buttons - back/forward offer ability to navigate thought diagram history. This are bind to context menu options
- reset view - refresh the diagram view
- zoom in/out buttons
The diagram area contains the diagram representation of the GTM model. The diagram is represented on 2 levels containing sub-diagrams for CMU and also for ATOM, TIM, TOM and TBU specific to each cluster which can be accessed when the when the cluster 0 is enabled for cmu diagram respective as long as a channel for ATOM, TIM, TOM and TBU is enabled. The sub-diagram can be accessed by double-clicking on the specific block if it is blue, indicating that it is enabled.
The diagrams can be moved by using click pressed and drag action. The zoom in/out can be done also by ctrl+scroll wheel.
|