Introduction
The S32
Configuration Tools set is a suite of evaluation and configuration tools that help you
from initial evaluation to production software development. The following tools are included:
| Name | Description |
| Enables you to configure the pins of a device. Pins tool enables you to create, inspect, change, and modify any aspect of the pin configuration and muxing of the device. | |
|
|
Enables you to configure initialization of the system clock (core, system, bus, and peripheral clocks) and generates the C code with clock initialization functions and configuration structures. |
| Peripherals Tool | Enables you to configure the initialization for the S32 SDK drivers. |
| IVT Tool | IVT Tool allows configuration and generation of the Image Vector Table using the format and constraints specified in the BootROM reference manual. |
| DCD Tool | DCD tool is used to generate the Device Configuration Data (DCD) image using the format and constraints specified in Boot ROM reference manual. |
| DCF Tool | DCF tool is used to generate the Device Configuration Format image using the format and constraints specified in Boot ROM reference manual. DCF tool is replacing DCD tool for S32K3 family processors. |
| QuadSPI Tool | QuadSPI tool allows the configuration of the parameters and the required details that are programmed in flash memory. The result configuration is exported in a .bin file that is imported in the QuadSPI parameters field of the IVT tool. |
| DDR Tool | DDR Tool provides a user-friendly graphical interface to configure DDR Controllers. |
| eFUSE Tool | eFUSE tool provides an intuitive graphical interface for writing/programming the OTP (One Time Programable) bits by software. |
| GTM Tool | GTM tool allows the configuration of the Generic Timer Module, with the objective of generating source code necessary to output PWM signals or analyze incoming waveforms. |