IVT Memory Layout
Offers a graphical representation of the memory, for a better view of the IVT segments and IVT image position.
The start address and end address are displayed for each segment. Free space is also highlighted and all the segments are scaled in respect to the total size of the used memory.
|
For a consistent representation, avoiding confusion, addresses are always displayed in HEX format and size is displayed in DECIMAL format.
Overlapping segments are detected and highlighted in the Memory Layout, for an easier conflict resolution.
|