Mouse actions in diagram
You can perform the following actions in the Clock diagram view.
- Position the mouse cursor on the element to see the tooltip with the information on the clock element such as status, description, output frequency, constraints, and enable/disable conditions.
- Single-click on output frequency or scale to change output frequency or scale.
- Single-click on lock to remove the lock.
- Single-click on a selected Clock source to display a dropdown menu for enabling or disabling the source.
- Single-click on a selected
Clock selector to display selector input options.
Figure 1. Clocks mouse actions in diagram
- Right-click on the element, component, or clock output to see a pop-up menu
with the following options.
- Edit settings of: {element} – Invokes the floating view with the settings for a single element.
- Edit all settings – Invokes the floating view with all the settings for an element.
- Edit settings on the path to: {clock output} – Invokes the floating view with the settings for all elements on the clock path leading to the selected clock output.
Figure 2. Floating view