Overlay Charts
Offers an interactive representation of the Diag margin test results, displaying the overlapped eye contours.
- Vertical axis contains Vref values in Volts.
- Horizontal axis contains Delay coordinates in either UI or picoseconds, depending on the user’s choice. Values are automatically converted to the selected unit of measurement.
|
The chart can display all or any subset of the available data lines. This can be
configured through:
- The interactive legend from the right, which allows enabling/disabling any series on the graphic, as well as highlighting a specific one by hovering over its name.
- Checkboxes below the chart for toggling an entire byte at a time.
|
The zoom function is available on the graph by drawing a rectangle for the area to be zoomed in and double-clicking to reset to the original format. To easily identify the position of a particular point, the coordinates are displayed after passing the cursor over that point.
|
The Content in Overlay Charts can be exported in HTML format by pressing the button in the upper right corner.
|