Pins routing principle
The Pins tool is designed to configure routing peripheral signals either to pins or to internal signals.
Internal signal is an interconnection node that peripheral signals can be connected to (without any pin interaction). Connecting two peripheral signals to an internal signal makes an interconnection of these two peripheral signals.
This routing configuration can be done in the following views:
- Pins
- Peripheral Signals
- Package
- Routing Details