To access the menu, right-click on the clock output in the clocks view or in the diagram.
Lock/Unlock – Removes a lock on the frequency which enables the tool to change
any valid value that satisfies all other requirements, limits, and constraints.
Find Near Valid Value – Tries to find a valid frequency that lies near the
specified value, in case the tool failed in reaching the requested frequency.
Advanced resolver for {Clock output} - Invokes more advanced search for the valid
settings that fulfills the requirements. It may take significant time so a progress dialog
is shown. If the resolver is not successful, the user is informed about it. This command can
alter clock selectors and modify various other clock settings on the clock path. If the
result is not satisfactory, use the UNDO command to return to the original
state.
Edit settings of: {element} – Invokes the floating view with the settings for a
single element.
Edit all settings – Invokes the floating view with all the settings for an
element.
Edit settings on the path to: {clock output} – Invokes the floating view with the
settings for all elements on the clock path leading to the selected clock output.
Figure 1. Pop-up commands for outputs in the clocks table view
Figure 2. Pop-up commands for outputs in the clocks diagram