The tool validates the settings and problems and errors are reported in the Problems view.
If there is an error related to the setting or component, an error decorator is shown
next to the element containing an error. Figure 1. Error decorators
In the case of a dependency error, a quick-fix button is displayed. Figure 2. Quick fix 1
Right-click the button to display a list of issues, then left-click the issue to display
possible solutions. Figure 3. Quick fix 2
The
problem can be quickly fixed even when reported from a table cell as the context menu
contains the list of possible quick fixes (see register initialized SCTimer, for example
LPC54114 Resources->Outputs setting).