Problems view
The Problems view displays issues in individual tools and in the interdependencies
between the tools.
|
To open the Problems view, click the Show Problems view button in the Toolbar, or select Views > Problems from the Menu bar.
The Problems table contains the following information:
| Item | Description |
|---|---|
| Level | Severity of the problem: Information, Warning, or Error. |
| Resource | Resource related to the problem, such as the signal name, the clock signal. |
| Issue | Description of the problem. |
| Origin | Information on the dependency source. |
| Target | Tool that handles the dependency and its resolution. |
| Type | Type of the problem. It is either the validation checking dependencies between tools, or a single tool issue. |
Every issue comes with a context menu accessible by right-clicking the table row. Use this
menu to access information about the problem or to apply a quick fix where applicable. You can
also copy the rows for later use by right-clicking the row and selecting Copy or by
using the Ctrl+C shortcut. You can use the Ctrl+left-click shortcut to add
additional rows to the selection.
Note: A quick fix is only available for problems highlighted
with the "light bulb" icon.