QuadSPI Export Image

This option allows the user to export the configured QuadSPI binary image.

There are two exportable formats available:
  • Binary format
  • C format

The import/export options can be found in the left side of QuadSPI View.

Figure 1. QuadSPI General Parameters

When clicking export, a window will appear on the screen that will allow the user to preview the content of the image and export the code in the desired format.

Figure 2. QuadSPI Export C format
Figure 3. QuadSPI Export binary format

The sections of the exported binary image are highlighted using different colors and hovering over each byte will display the image section name that the byte is part of.

After the format has been chosen, user can click OK button and a file dialog chooser will appear in order to select the location where the QuadSPI image will be saved.