Setting states and markers

The following states, styles, and markers reflect the information shown in the settings’ rows in the settings tables (clock sources, output, details, or individual).

Table 1. Setting states and markers
State/Style/Marker Icon Description
Error marker Indicates that there is an error in the settings or something related to it. See the tooltip of the setting for details.
Warning marker Indicates that there is a warning in the settings or something related to it. See the tooltip of the setting for details.
Lock icon Indicates that the settings (that may be automatically adjusted by the tool) are locked to prevent any automatic adjustment. If the setting can be locked, they are automatically locked when you change the value. To add/remove the lock manually, use the pop-up menu command Lock/Unlock.
Note: The clock element settings that cannot be automatically adjusted by the tool keep their value as is and do not allow locking. They are: clock sources, clock selectors, and configuration elements.
Yellow background Indicates that the field is directly or indirectly changed by the previous user action.
Gray text Indicates that the value of setting does not actively influence the clock. It is disabled or relates to an inactive clock element. For example, on the clock path following the unavailable clock source or disabled element. The frequency signal also shows the text “inactive” instead of frequency. The value is also gray when the value is read-only. In such a state, it is not possible to modify the value.