Settings Editor
You can edit peripheral component settings in the Settings Editor. Open editors are shown in the central area of the screen, each with its own tab. Multiple editors can be opened at the same time. Changes done in the editor are immediately applied and kept even if the settings editor is closed. Settings that are disabled are highlighted in gray. In case that a component instance is disabled, all settings are highlighted in gray. Tooltips are displayed for all enabled settings when the mouse cursor is placed at settings.
To open Settings Editor, do the following:
- Double-click the component instance in the Peripherals or Components view to display component instance settings.
- Left-click the component in the Components view to display global settings of the component.