Toolbar

The toolbar is on the top of the window and includes buttons/menus of frequently used actions common to all tools. See the following sections for more information.
Table 1. Toolbar
Item Description
Config Tools Overview Open the Overview dialog with information about currently used tools.
Show Problems View Open the Problems view.
Update Code Open the update dialog allowing you to update generated peripheral initialization code directly within the specified toolchain project.
Generate Code Regenerate source code when the "Enable Code Preview" preference is disabled.
Manage SDK Components Manage SDK Components in the project. For more details, see Add SDK drivers to project
Functional group selection Select a functional group. A functional group in the Peripherals tool represents a group of peripherals that are initialized as a group. The tool generates a C function for each function group that contains the initialization code.
Call from default initialization Set the current functional group to be initialized by the default initialization function.
Functional group properties Open the Functional group properties dialog to modify name and other properties of the function group.
Tool selection Display icons of individual tools. Use them to switch between tools.
Undo/Redo Undo/Redo last action.

In addition, the toolbar may contain additional items depending on the selected tool. See the chapters dedicated to individual tools for more information.