User templates
You can export and store the current configuration as a user template for later use as a reference configuration file.
The exported template is available in the New Configuration wizard and can be used to
create a configuration. You can also define custom labels for pins or identifiers prefixes for
#define in the generated code. You can export the configuration by
selecting, in the Menu bar, File > Export > Tools Configuration
> Export Configuration as Template.
Note: The templates are stored in at the following location on your local hard disk:
{$user}/.nxp/{tools_folder}/{version}/templates.