Using DDR view

This chapter explains how to use DDR View to configure the DDR for a certain DRAM and board layout.

Configuring the DDR starts with selecting the memory type and based on it, DDR View will display a set of configurable parameters like Frequency, Number of Channels, Number of Ranks, DRAM Configuration, Board Settings options, etc.

Figure 1. DDR view