|
|||||||||
| PREV CLASS NEXT CLASS | FRAMES NO FRAMES | ||||||||
| SUMMARY: NESTED | FIELD | CONSTR | METHOD | DETAIL: FIELD | CONSTR | METHOD | ||||||||
public interface Cache<T>
The Cache interface is used to represent a cache
that will store key value pairs. The cache exposes only several
methods to ensure that implementations can focus on performance
concerns rather than how to manage the cached values.
| Method Summary | |
|---|---|
void |
cache(java.lang.Object key,
T value)
This method is used to insert a key value mapping in to the cache. |
boolean |
contains(java.lang.Object key)
This is used to determine whether the specified key exists with in the cache. |
T |
fetch(java.lang.Object key)
This method is used to get the value from the cache that is mapped to the specified key. |
boolean |
isEmpty()
This method is used to determine if the cache is empty. |
T |
take(java.lang.Object key)
This is used to exclusively take the value mapped to the specified key from the cache. |
| Method Detail |
|---|
boolean isEmpty()
void cache(java.lang.Object key,
T value)
key - this is the key to cache the provided value tovalue - this is the value that is to be cachedT take(java.lang.Object key)
key - this is the key to acquire the cache value with
T fetch(java.lang.Object key)
key - this is the key to acquire the cache value with
boolean contains(java.lang.Object key)
key - this is the key to check within this segment
|
|||||||||
| PREV CLASS NEXT CLASS | FRAMES NO FRAMES | ||||||||
| SUMMARY: NESTED | FIELD | CONSTR | METHOD | DETAIL: FIELD | CONSTR | METHOD | ||||||||