The Analysis Results view shows and manages collected traces.
The main features of the Analysis Results view are: organizing logic of trace and profiling results, enable/disable links towards profiling viewers, save/rename/delete results, expand all/collapse all results, and refreshing the view.

| Button | Description |
|---|---|
| Refresh | Refreshes the view and rescans all output folders for trace and analysis results |
| Expand all | Expands all nodes in the tree |
| Collapse all | Collapses all nodes in the tree |
| Select custom results folder | Allows to select a custom folder to scan for trace results |
The Analysis Results view can also show the results from more folders. Each platform
configuration available in
.metadata/.plugins/com.freescale.sa/platformConfig/ folder is checked for
the path specified towards the set of results. All sets of trace and profiling results found
in those paths will appear in the Analysis Results view. All the trace results available in workspace/.AnalysisData are displayed in Analysis Results view.
To configure the view to display trace data of another custom results folder that does not belong to any platform configuration inside the workspace:
The Custom results folder dialog gets displayed.
The SA Results Folder Selection dialog opens.
The path to the custom folder for which the trace needs to be collected gets added under the Path field.
To configure the results folder for a platform configuration, specify the Results folder location available in the Trace Configurations dialog box as shown in the below figure. The collected trace using the Platform configuration will be saved in the specified folder.

To view the collected trace data, click on the links of profiling results from the Analysis Results View: