Click on the Timeline link from Analysis Results view to view timeline data.

Timeline viewer has a tabbed interface. A tab for each source (usually a core) is created automatically. Each tab has its independent timeline plot with its own setup of groups and time unit. The timeline viewer can be controlled using the toolbar. The timeline data displays the functions that are executed in the application and the number of cycles each function takes when the application is run. The Timeline viewer shows a timeline graph in which the functions appear on y-axis and the number of cycles appear on x-axis. The green-colored bars show the time and cycles taken by the function.
The Timeline viewer has the following buttons:
Edit Groups: Allows you to customize the timeline according to the requirements. You can change the default color of the line bars representing the functions to differentiate. You can add/remove a function to/from the timeline. To perform these functions, select Edit Groups. The Edit Groups dialog box appears.

You can perform the following operations in the Edit Groups dialog box: